Camozzi and the “Automation Passport” at SPS


May 20 2016

Camozzi is one of the sponsors of this competition

In occasion of this year’s edition of the SPS IPC DRIVES Italy, we welcome back the competition called “Automation Passport”, an initiative that is sponsored by 4 companies this year: Balluff (Hall 3, Stand A010), Camozzi (Hall 3, Stand F002), iMAGE S (Hall 2, stand M026) and Rittal (Hall 2 Stand J022/K022).

 

The prize money at stake is very abundant: the first number drawn will receive a travel voucher for the amount of 3.000€, while the second will obtain an Apple voucher for the amount of 650€ and the third an Eataly voucher for the amount of 350 €.

 

The initiative is open to all visitors of the exhibition that are not directly connected with the promoting companies and has an extremely simple method of participation: the visitors only have to collect the "Automation Passport" at the special stand in Hall 4, fill it in completely, bring it to the 4 stands of the promoting companies to get a stamp and put the stamped part in the special box in Hall 4. The extraction of the fortunate winners will be performed within 30 June 2016.

For more information, please visit the site www.passaportoautomazione.it