How to reach us



Camozzi S.p.A.
Headquarters & Offices

Via Eritrea 20/I
25126 - Brescia - Italy
Tel. +39 030 37921
Fax +39 030 2400464
By car: on the A4 highway, (Milano-Venezia), exit at BRESCIA Ovest gate: you are less than 10 minutes from Camozzi headquarters.
By plane: even if the two closest airports are Bergamo "Orio al Serio" and Verona "Catullo" you will be likely to land in Milano "Linate" airport. From there you can either take a taxi (about 1h time and huge amount of money!) or get to the Milano Central Station from where you can take a train (see below); from "Linate" to Central Station you can take a taxi (about 20 minutes) or use public transportation which is less expensive but not very frequent (take into account one hour).
By train: trains on the Milano-Venezia line are quite frequent (one no-stop train each hour) and bring you to Brescia in about 50 minutes; from Venezia the trip can take you less than 2 hours. In both cases get off at Brescia station.


Camozzi S.p.A.

Via Borrine, 23/25
25080 Polpenazze d.G.
Brescia - Italy
Tel. +39 0365 674046
Fax +39 0365 674306
By car: on the A4 highway, (Milano-Venezia), exit at Desenzano gate: at the 13th km of the Desenzano-Salò road, close to the Moniga round, torn left direction Soiano del Lago/Polpenazze and go straight on for about 1 km.
By plane: Nearest airport: Valerio Catullo (Verona) at 35 km or Montichiari Airport (Brescia) at 30 km.
By train: nearest railway station: Desenzano.


Camozzi S.p.A.

Via Moretto, 39
25065 Lumezzane S.S.
Brescia - Italy
Tel. +39 030 8920521
Fax +39 030 829341
By car:
From: Milan
- A4 highway (72 km) direction Venezia
- Exit at Brescia-Ovest gate
- Main road S510 direction Iseo
- Exit on local road direction Lumezzane

From: Roma
- A1 highway (400 km)
- A22 highway direction Cerese (86 km)
- A4 highway direction Castiglione S. (61 km)
- Exit at Brescia-Ovest gate
- Main road S510 direction Iseo
Exit on local road direction Lumezzane
By plane: Nearest airport: Valerio Catullo (Verona) at 35 km or Montichiari Airport (Brescia) at 30 km.
By train: nearest railway station: Brescia.